Helmholz

Helmholz Logo Authorised Partner Logo

Whether memory cards for SIMATIC S7-1200/1500, PROFINET and Ethernet connectors, robust managed PROFINET switches, or gateways for effortless system networking, with the experienced manufacturer Helmholz you get top quality, made in Germany. Available now at brilliant prices from Automation24.

Contact

Do you have any questions?

The trained support team at Automation24 looks forward to advising you personally.

phone 00800 24 2011 24

Icon Mail info@automation24.com



Who is Helmholz?

Helmholz is an international expert in industrial networks and PROFINET.

The story of how it came to be goes back to 1988. In an engineering office for software and plant commissioning in Erlangen-Dechsendorf, Manfred Helmholz and his two employees pursued the idea of optimising automation tasks through clever yet simple system solutions.

Helmholz systems – made in Germany through every step of production

The topics of big data and industry 4.0 are the company's driving force. The result: Helmoholz develops increasingly efficient, contemporary products that are in line with the market and facilitate modern industrial operations.

All three of the following steps in the production process take place in Germany:

  • development
  • assembly
  • quality assurance

The company has been ISO 9001:2015 certified since 1999 and guarantees compliance with high quality standards and valid EU directives. You can rely on Helmholz systems made in Germany!

Helmholz products in stock now on Automation24 at the best prices

At Automation24 you can find Helmholz products from the Industrial communication technology category, for the simple networking of machines. The RJ45 PROFINET connectors and RJ45 Ethernet connectors feature EasyConnect® quick-connection technology, which avoids connection errors. The connector is available in versions with a 90°angle or a 180° cable outlet.

The lightweight yet robust managed PROFINET switches are available in numerous designs. Beginning with compact switches with 4 ports, there are also options with 8, 10, and 16 ports. The connection options here are an RJ45 PROFINET connector, fibre optic, or an M12 PROFINET connector. One major advantage of the PROFINET switch with the M12 connections is the IP67 protection rating. As a result, the product can also be used without an industrial enclosure. If network issues still occur, Ethernet diagnostic tools help quickly identify sources of errors, such as cable breaks or misconfigurations, and ensure system availability.

For reliable control cabinet monitoring, Automation24 offers an innovative solution with the compact Cabinet Guard from Helmholz for control cabinet monitoring. It enables monitoring of the control cabinet door as well as key environmental conditions such as temperature, humidity, air pressure, and vibrations. This allows changes and critical operating conditions to be detected at an early stage, helping to ensure high system availability. The Cabinet Guard therefore provides an ideal foundation for condition monitoring and retrofit projects.

When it comes to industrial communication technology, gateways are absolutely essential. They establish the connection between machines that operate with different networks and thus enable communication between them. Automation24 offerw Gateways from Helmholz that allow you, for instance, to connect systems with different communication standards such as PROFINET, PROFIBUS, EtherNetIP, CAN Bus, ModbusTCP and MQTT. NAT gateways/firewalls are also available to protect networks against external access. Suitable gateways can be found within the PROFINET / PROFIBUS Gateways, Ethernet / EtherCAT Gateways, CAN Bus Gateways, Modbus Gateways and MQTT Gateways categories.

Furthermore, Helmholz memory cards from the control systems section are cost-effective components for the SIMATIC S7-1200 or the S7-1500 series from Siemens.

If you want to optimise your industrial communications processes and find sustainable solutions at the same time, then opt for Helmholz systems today. Order the products of your choice now from Automation24 and prepare to be impressed! We will ship your goods within 24 hours.


You may also be interested in these topics from the Automation24 Knowledge Corner.

Industry 4.0

Wiring of control cabinets

The Automation24 range offers a wide selection of products for the easy wiring of control cabinets. [...]

Find out more

Grenzstandmessung

From the sensor to the control box

At Automation24, you will find a comprehensive range of products for your installations. [...]

Find out more

Grenzstandmessung

Condition monitoring

Imagine an important machine in your production cycle suddenly breaks down - without warning. […]

Find out more