Selec

Selec logo Selec knows that high quality doesn't necessarily have to come with high prices. At Automation24, you can purchase the manufacturer's high quality and reliable products from the industrial controls, measurement and control technology, and power supply categories, at discounted prices. See for yourself today!


Selec: your specialist for industrial automation technology

Selec Controls Pvt. Ltd. is a company that was founded in 2000 in India, specialising in industrial automation technology.

The manufacturer impresses with high-quality industrial controls, reliable protection relays, measuring devices, and its measurement and control technology, among other products. As such, Selec is the market leader in India, on account of its versatile timer relays, time switches, and temperature controllers.

In 2006 the company began to expand, commencing with the establishment of an international distribution network.

This lead to the foundation of the American subsidiary company, Selec Controls USA Inc in 2008. In 2010 came another milestone, with the opening of the German sales office, Selec GmbH.

Alongside India, Germany, and the USA, other countries in Europe, Asia, and Africa now benefit from Selec solutions. The success speaks for itself, as the worldwide expansion continues to progress.

Selec: reliable & high product quality

Selec places great value on

  • the meticulous manufacture and testing of its products,
  • ensuring exceptional quality
  • and the fulfilment of customer requirements.

The high quality standard to which SELEC products ascribe is confirmed by their certification in accordance with ISO 9001.

What's more, most of the products from Selec bear the internationally recognised UL and CE seals of approval, thus attesting to the fulfilment of applicable safety standards, as well as European standards and directives.

To ensure the careful production of assemblies and plastic components, the company runs modern production facilities in India.

Innovative products from Selec at discounted prices, at Automation24

At Automation24 you will find a diverse selection of high-quality Selec products, at particularly appealing prices.

You can thus purchase both an analogue and a digital timer relay from the industrial controls category, featuring a host of functions and simple DIP and rotary knob control.

Furthermore, here you will also find products from the current monitoring category, for the effective protection of plants against under and overload, as well as voltage-monitoring to detect at an early stage when voltage limits are exceeded, available for single or 3-phase systems. For temperature current monitoring, you can rely on the various PID temperature controllers from Selec, featuring different display sizes.

Also available within the industrial controls range are two digital time switches, with which you can programme ON and OFF switching processes. Here you can choose between a clock with daily/weekly functions, and a version with astronomical functionalities.

You can also find a wide range of process displays / counters within the measuring & regulation technology category.

Here you can select instrument transducers for detecting high primary currents. You can choose between rectangular current transformers for busbars and round CBCT summation current transformers for earth fault relays.

Digital ammeters from Selec enable the measurement of direct and alternating currents, and the representation of the measurement values via the 4-digit LCD display. They also visualise the values in analogue form, by means of a bar display.

For the detection and visualisation of voltages, on the other hand, there are meters with a 3-digit LCD display.

If you want to assess your system status and network quality, multifunction meters are a good option, as they measure diverse parameters such as voltage and current, and thus enable the drawing of conclusions.

With Selec switched-mode power supplies, Automation24 has also thought of the suitable power supply. You can purchase Din-rail mounted power supplies, 24 V DC and Din-rail mounted power supplies, 12 V DC.

Thanks to Selec, you can ensure safe and reliable operating processes, without blowing the budget. See for yourself today!

Still have unanswered questions regarding the products from Selec or other manufacturers? The competent support team at Automation24 would be happy to assist you. Simply get in contact.