WAGO

WAGO Logo Authorized Partner Logo

Do you want to be on the safe side and minimize dangers such as loose contacts, short circuits or electric shocks as well as faulty signal transmissions in your application? Then our product selection from the manufacturer WAGO, the specialist for connection technology, is just right for you.

Contact

Product not found? We are happy to help you — also with ordering WAGO products beyond our webshop portfolio.

Please contact us for prices and availability:

phone 00800 24 2011 24

Icon Mail  info@automation24.com



WAGO – Always on the safe side

The family owned company WAGO, founded in 1961, with its headquarters in Minden (North Rhine-Westphalia), a central warehouse in Sondershausen and a large number of sales locations, impresses worldwide with products from the fields of electrical connection technology and automation. WAGO is never satisfied with what is already there, but continually strives to develop innovative products that are not only characterized by high quality, but above all are easy and safe to use. Creativity and perseverance are essential for future innovative developments to be possible.

WAGO practices environmentally responsible behaviour during production. By using geothermal energy and rainwater as well recovering heat, the ecological idea is implemented. WAGO is convinced that long-term success is only possible through sustainable action.

WAGO – strong connection

The success so far speaks for itself. WAGO is particularly known for its PUSH WIRE plug-in terminal technology in box terminals, which was developed in 1947 and enables the fast and uncomplicated connection of solid conductors. Another innovation followed in 1977 with the CAGE CLAMP tension spring technology. The connection with tension spring terminals is a safer alternative to screw connections, since the risk of loose contact, short circuit or electric shock is minimized. There are now various spring clamp systems that are constantly being developed to meet a wide range of requirements.

WAGO products have become indispensable in industry and are part of the standard repertoire for many companies.

WAGO at Automation24

Automation24 offers a variety of products from automation technology at incredibly low prices. These include, for example, connection terminals for all types of conductors from the area of connection technology from the manufacturer WAGO, the world market leader for spring clamp technology. Whether 2, 3 or 5-pole terminals – you will find it here.

You can also purchase the signal conditioners as well as isolation amplifiers from WAGO from the category Measuring & regulation technology. These ensure reliable and error-free transmission of signals.

All WAGO products meet the requirements of DIN ISO 9001, ISO 14001 and IRIS.

You can also find the right WAGO products for your application. At Automation24, you can get connection technology for a low price!