Condition monitoring: condition-based maintenance & predictive maintenance

Imagine an important machine in your production cycle suddenly breaks down - without warning. Production comes to a standstill and valuable hours pass while you wait for the expensive repair or even a replacement. A nightmare, isn't it? Yet, this is a harsh reality for many companies. But it doesn’t have to go that far!

To prevent such situations, modern companies now rely on condition monitoring (CM), the basis for condition-based maintenance (CBM) and predictive maintenance (PdM).


Keyvisual Condition Monitoring

Would you like to start directly with condition monitoring?

Directly to the condition monitoring solutions

Would you like a personal consultation?

Call free of charge 00800 24 2011 24


Condition monitoring is a requirement for modern maintenance measures in industrial processes

Especially in the age of Industry 4.0, it is more important than ever to rely on smart systems that enable proactive action and contribute to increasing production efficiency.

To ensure that the terms "condition monitoring", "condition-based maintenance" and "predictive maintenance" don't just remain abstract buzzwords for you, this Automation24 guide explains how these concepts work in concrete terms, how you can benefit from them and why you shouldn't wait any longer to optimise your industrial processes and take them to the next level.

IO-Link Grundlagen Keyvisual
Fig. 1: From reactive maintenance to predictive maintenance

What is condition monitoring?

Condition monitoring covers the condition monitoring of machines and systems and is a fundamental pillar of Industry 4.0.

In this context, the so-called "digital shadow" is used, through which the current state of a system can be virtually represented. The digital shadow refers to process data generated by machines while they are in operation. These can incluse physical parameters such as temperature, vibration, oscillation, pressure, humidity and electrical signals or even the oil quality. This allows the condition of these machines to be checked and analysed at any time, typically in real-time or at predetermined intervals.

This enables early detection of potentially critical conditions and the taking of appropriate measures, thus systematically preventing failures and downtimes. Condition monitoring is therefore a central element of modern maintenance strategies.

What components does condition monitoring consist of?

All the essential components for solid condition monitoring are most likely already in your systems today. This can look like this, for example:

1. Data recording: Sensors record relevant machine and process data. These can be the following, for example:

  • Vibration sensor: Warns if machine vibrations deviate from the standards.
  • Inductive sensor: Detects changes in the distances between components using the sensing range for early bearing wear detection.
  • Ultrasonic sensor: Indicates errors in the process if there is no sound reflection.

2. Data transmission: IO-Link and similar protocols ensure continuous communication.

3. Programmable logic controller (PLC): Provides the sensor data to the network.

What advantages does condition monitoring offer?

Efficient condition monitoring offers you numerous benefits for your business, including

  • Early detection of machine problems: Damage or wear and tear are recognised before they lead to expensive breakdowns.
  • Preventive elimination of the cause: A defective part can be repaired or replaced before damage occurs.
  • Wear reduction: Proactive intervention also prevents wear on other machine parts.
  • Increased efficiency: Optimised maintenance intervals avoid unnecessary maintenance work and increase machine availability.
  • Cost reduction: Targeted measures minimise expensive repairs and production downtime and reduce operating and maintenance costs.
  • Increased safety: Monitoring sensitive system components reduces the risk of accidents.

Practical overview of common parameters for condition monitoring

Parameters: Function:
Vibration Detection of mechanical faults, such as bearing faults and balancing. Analysis tools can be used to predict when a critical condition will be reached that will lead to a failure.
Temperature Detection of temperature deviations to identify imminent sensor failures due to exceeding the temperature resistance limit. The time for maintenance or sensor replacement can be predicted based on analysed temperature trends.
Flow rate Monitoring the flow of liquid or gas to detect leaks or blockages.
Pressure Measurement of pressure changes that adversely affect the compressive strength limits of the components used and enable a forecast of impending faults.
Ultrasound Detection of objects or positions by reflection of ultrasonic waves. Missing or changing reflections can indicate process problems or machine malfunction.
Fill level Monitoring of tank levels to warn of the time of an overflow or dry run.
Conductivity Measuring the conductivity of lubricants to detect water build-up or contamination that can affect lubricant performance and system condition. By analysing conductivity trends, the optimum time to treat or replace the lubricant can be predicted.
Moisture Monitoring of moisture in machine components to predict when corrosion will occur on critical components and when maintenance should be carried out.
Acoustics Identification of abnormal noises that indicate worn bearings or loose components. Analysing the acoustic signals enables maintenance requirements to be predicted at an early stage before safety-critical faults occur.

What is predictive maintenance (PdM)?

While condition-based monitoring (CBM) already provides an efficient basis for monitoring the condition of the machine, predictive maintenance (PdM) goes one step further and uses the data collected by CBM in combination with more advanced analysis methods to accurately predict the optimum time for maintenance.

"Predictive maintenance" (PdM) aims to predict when maintenance will be required - before an acute malfunction occurs and the industrial process comes to a standstill.

With periodic maintenance, maintenance is carried out at fixed times regardless of the system status, which usually results in unnecessary downtime. While reactive maintenance addresses issues only after critical deviations or impairments occur, predictive maintenance acts earlier, proactively preventing anomalies and failures.

Compared to traditional maintenance strategies, predictive maintenance focuses on preventive rather than periodic or reactive maintenance measures.

IO-Link Grundlagen Keyvisual
Fig. 2: The three levels of predictive maintenance

What advantages does predictive maintenance offer?

As predictive maintenance is an advanced version of modern maintenance strategies, a separate chapter is dedicated to the numerous short-term and long-term benefits.

  • Optimised maintenance management: Time, a valuable resource, is now used exclusively for necessary, plannable maintenance intervals - unexpected faults are eliminated. If a sensor is defective, it can even be replaced during operation thanks to modern communication technologies such as iO-Link, provided an identical sensor takes its place.
  • Maximising production efficiency and machine performance: Early identification of declining machine performance and proactive maintenance optimises the performance and service life of the machines and minimises downtimes. Plant availability is increased and the process result is consistently maintained at a high level of quality.
  • Increased efficiency: Maintenance costs are no longer incurred in the event of sudden malfunctions, but only for planned and cost-efficient maintenance. Unnecessary and costly process downtimes are a thing of the past.
  • Increased safety: Early repair of defective system components prevents potentially dangerous machine faults, thereby preventing safety-critical situations and protecting both machines and applications.

The parameter data is transmitted to local edge computing devices or to centralised cloud-based systems, where it is collected and processed using innovative analysis tools such as moneo. This allows failures to be predicted at an early stage and appropriate maintenance measures to be planned.

By utilising big data, machine learning and artificial intelligence (AI), the analysis tools continuously "learn" from the collected data and deliver increasingly precise forecasts. With the help of advanced data modelling, patterns and correlations are derived from these large amounts of data over time, making it possible to identify failures and maintenance requirements at an early stage. As a result, the failure probabilities initially calculated by the algorithm adapt to changing conditions and are recalculated accordingly. In this way , the predictions are always based on the actual prevailing conditions.

Users can also actively contribute to "teaching" the analysis tool by enriching the analysis and forecasting models with annotated data and specific feedback. Annotated data contains important additional information, such as downtimes or operating states, which help to further increase the accuracy of the model.

In order for maintenance measures to be truly "predictive", it is imperative that the data is transmitted in real time. This is where advanced technologies such as IO-Link come into play, enabling seamless communication between sensors, actuators and controllers. These ensure that all relevant data is processed quickly and reliably so that maintenance can be carried out before faults even occur.

In addition to failure prediction, which is based on the parameters processed by analysis tools, "digital twins" can also be used - virtual images or models of machines and systems that simulate their condition and functionality in real time.

The use of a Computerised Maintenance Management System (CMMS) is suitable for managing and planning the maintenance measures derived from the forecasts and simulations. With this system, maintenance actions can be efficiently planned, prioritised and documented, optimising the handling and transparency of the entire maintenance process.

Difference between condition monitoring, condition-based maintenance and predictive maintenance

Many wonder about the differences between "Condition monitoring", "Condition-based maintenance" and "Predictive maintenance".

"Condition monitoring is purely the monitoring of the condition of machines. The respective maintenance strategies "condition-based maintenance" and "predictive maintenance" then utilise this data. The strategies differ depending on whether maintenance is subsequently planned based on this data (CBM) or whether the data is processed by software, algorithms or AI. The aim of both approaches is to react before a problem occurs.

To illustrate this, you will find a comparison of the two maintenance strategies below:

Criterion Condition based maintenance (CBM) Predictive maintenance (PdM)
Maintenance strategy Condition-based maintenance: Records and analyses the condition of machines in order to carry out targeted maintenance measures and avoid unplanned downtime. Predictive maintenance: Proactive component replacement before potential failures and malfunctions.
Maintenance frequency Demand-orientated frequency: Maintenance is carried out based on measured condition data instead of following fixed intervals. Maintenance at the optimum time: During a functioning operating process, but before an actual defect or machine downtime occurs.
Data sources Sensors and systems: Use of sensors such as vibration sensors, temperature sensors, acoustic indicators and other systems that provide operating data. Sensors and systems: also play a role in CBM, providing aggregated real-time data that is used in combination with historical operating data, machine learning models and AI-supported analyses. The comprehensive utilisation of the various data sources goes beyond pure real-time analysis.
Degree of complexity Low to moderate effort: Simple monitoring mechanisms and important system parameters (e.g. limit value monitoring). Moderate to high effort: Implementation of advanced analysis tools and algorithms, even though many tools are now available at low cost or free of charge.
Costs Low to medium initial investment: For sensor technology, but long-term savings through reduced downtimes and optimised maintenance plans. Systems are often already equipped with condition monitoring-capable systems that may not yet be utilised. Higher initial investment: For the integration of smart sensors, Industry 4.0-enabled components and analytics tools. Once the comprehensive infrastructure and data processing are in place, there are long-term benefits from preventive maintenance strategies that avoid downtime and increase operational efficiency.

How do you use condition monitoring?

In order to ensure smooth monitoring of your machines and systems, a number of technical requirements are necessary, but in many cases these can be easily implemented. Often, components that have already been installed already have the required functionalities and are simply not being utilised accordingly. If this is not the case, Automation24 explains the technical basics of condition monitoring right from the start.

What are the technical basics of condition monitoring?

  1. Sensors: Every condition monitoring solution is based on high-quality sensors that measure key parameters such as temperature, vibration, pressure or humidity in real time. For example, vibration sensors can detect minimal deviations from target values that indicate imbalances, bearing problems or the onset of material fatigue. These are supplemented by temperature sensors. These recognise sudden overheating and damage to motors or gearboxes and can therefore prevent them.
  2. Data analysis: The recorded data is transferred directly to a central data analysis platform, where it is analysed using modern algorithms. These algorithms identify patterns and anomalies that would be barely recognisable to a human observer. This creates a comprehensive picture of the machine's condition, which enables predictive maintenance and minimises unexpected failures.

IoT, digitalisation and real-time data transmission

Digitalisation has taken condition monitoring to a whole new level. Thanks to the integration of the Internet of Things (IoT), data from various sources can be merged and analysed in real time. One example: IoT-enabled vibration sensors are used to transmit measured values directly to a central control unit via a local network or the cloud. There, the data is immediately available for further processing.

Real-time data transmission is a key aspect of modern condition monitoring systems. It ensures that machine operators are informed about the current status of their systems at all times. To achieve this, technologies such as 5G networks and LPWAN (Low Power Wide Area Networks) are used, which enable reliable communication even with a large number of sensors and over long distances.

Abb. 3: Datenanalyse ist das Herzstück von Condition-Monitoring
Fig. 3: Data analysis is at the heart of condition monitoring

Data analysis: how intelligent monitoring works

Data analysis is the centrepiece of a condition monitoring system. This is where all the information collected by the sensors comes together. But how exactly does this process work?

Firstly, the data is recorded and pre-processed. Raw data is filtered and normalised to ensure that it is suitable for further analysis. Vibration sensors, for example, can deliver thousands of measurement points per second. Pre-processing removes irrelevant data such as ambient noise so that only the truly relevant information is forwarded.

In the next step, the cleansed data is analysed using artificial intelligence (AI) and machine learning (ML). Algorithms identify patterns that indicate a potential error. For example, an AI-supported model could recognise that a continuously increasing vibration indicates a bearing defect - even weeks before the defect actually occurs! Predictive maintenance thus provides you with reliable support and protects you from machine failures a lengthy time in advance.


Automation24 solutions for condition monitoring

In connection with condition monitoring, Automation24 offers you a wide range of different solutions from proven automation technology brands. As the selection is extensive, we would like to give you just a first flavour of what you can find in the range.

ifm Hauber Elektronik Siemens Schneider Electric Endress+Hauser WIKA TiTEC NOVUS Automation microsonic IO-Link Leuze IO-Link Equflow
PHOENIX-CONTACT IO-Link Metri Measurements Honsberg Datasensing Selec TELE +GF+ – Georg Fischer AG Wieland Electric Eaton PATLITE
Condition monitoring type Solutions Example of intended use Brands represented
Condition monitoring Vibration sensors Testing for vibration anomalies to detect irregular machine movements, rolling bearing damage and imbalances in drives. ifm, HAUBER
Variable frequency drives Detection of speed deviations that indicate a drop in motor performance. Siemens, Schneider Electric
Temperature transmitters Monitoring of exceeding and falling below predefined temperature limits that could impair the functionality of machines or components. ifm, Endress+Hauser, WIKA
Pressure sensors Detection of pressure drops or pressure peaks that indicate leaks, blockages or defective components. ifm, Endress+Hauser, WIKA, TiTEC
Volumetric flow meters Detection of irregular flows of liquids or gases that may indicate leaks or blockages in the system. ifm, Endress+Hauser, Equflow, Metri Measurements, Honsberg
Humidity sensors Accumulation of moisture, which reduces the quality of food and favours the formation of rust and corrosion on components. TiTEC, NOVUS Automation
Ultrasonic sensors Used, among other things, in applications such as level measurement, object detection, object counting, or quality control by contactlessly detecting objects or positions. ifm, Endress+Hauser, microsonic, Datasensing
Voltage monitoring Check for overvoltages and undervoltages that cause sub-optimal operating conditions. Schneider Electric, Selec, TELE
Consumption measurement Compressed air meters Detection of the smallest deviations in the consumed quantities of compressed air, volume flow and temperature, which can indicate inefficient operation, leaks or waste of resources in the system. Schneider Electric, Selec, TELE
Electromagnetic flow meters Monitoring of water consumption based on the measured flow rate, volume and medium temperature; ideal for cooling circuits and the waste water industry. ifm, Endress+Hauser, Georg Fischer
Laser sensors Detection of altered distances and movements, which can be a sign of wear, deformation and misalignment. ifm, Datalogic, Leuze
Evaluation units Speed monitors Detection of setpoint deviations on conveyor drive shafts based on frequency and speed. ifm, PHOENIX CONTACT
Standstill monitors Detection of underspeed or standstill on drives, motors or shafts. Schneider Electric, PHOENIX CONTACT, Wieland
Process displays Display of actual values of physical depth/Width and detection of limit value violations to provide early warning of potential problems or malfunctions in the system. Endress+Hauser, WIKA, NOVUS Automation
Timer relays Monitoring of changed switch-on and switch-off delays of signals in order to detect anomalies or malfunctions in the system. Schneider Electric, Selec, TELE
Control monitor for temperature sensors Monitoring of minimum or maximum temperatures in order to recognise deviations at an early stage. ifm
Control monitor for flow sensors Monitoring of flow, temperature or wire breakage, especially in confined spaces and for ATEX applications. ifm, NOVUS Automation, Georg Fischer
Signal towers Visual and possibly also acoustic signalling for faster error detection. Eaton, ifm, PATLITE
blue line

Vibration sensors from Hauber

Vibration sensors from Hauber
  • ✔ Innovative technology thanks to decades of experience
  • ✔ New standards in vibration monitoring
  • ✔ Sensors with ATEX and IECEx certification available

Discover more

blue line

Implementation of condition monitoring and predictive maintenance

The implementation of condition monitoring (CM), whether as condition-based maintenance (CBM) or predictive maintenance (PdM), requires thorough planning and goal setting. It’s essential to clearly define at the outset why you want to integrate these strategies into the operational process and what you aim to achieve. Only once these fundamental questions are answered will you have laid the groundwork for successful implementation.

7 steps to realising a condition monitoring system

Condition monitoring enables companies to monitor systems more efficiently and extend the service life of their machines. However, installing such a system requires a structured approach to ensure that it works optimally. Here you will find a detailed step-by-step guide to implementing condition monitoring:

(1) Identification of critical machines in your system

Inventory:

  • Determine which machines or system components are essential for your operating process.
  • Decide which parameters (e.g. temperature, vibration and pressure) are indicators of the health of your machines.
  • Clarify which failures trigger chain reactions and cause a complete standstill, which would lead to considerable financial losses.

Objective: Decide whether the system should only be used for monitoring or also for predictive maintenance.

(2) Select suitable sensors

Select sensors based on the parameters to be monitored:

  • Vibration sensors: For bearings, gears or rotating machines.
  • Vibration sensors: For early detection of imbalances, resonance problems or mechanical damage to machines and drives.
  • Temperature sensors: For motors, cooling circuits or electronics.
  • Pressure sensors: For hydraulic or pneumatic systems.

An overview of all common parameters can be found in this table.

(3) Data generation and infrastructure development

Integrate a data acquisition system or analysis tool that is compatible with the solutions you use, such as moneo configure SA from ifm. Finally, connect this directly to your system components to collect and analyse real-time machine data centrally.

If you want to implement the predictive maintenance strategy, you need to set up an infrastructure that enables fast and reliable real-time data processing. This should consist of the following components, which complement each other perfectly:

  • Integration of alarm systems: Visual and/or acoustic solutions, such as signal towers, provide an additional level of security. They provide timely information about limit value outliers without the need to look at the monitoring software.
  • Communication technologies: Systems such as IO-Link, PROFINET and others ensure the seamless transmission of data.
  • Edge computing: Direct data processing on site minimises delays and relieves the burden on central systems.
  • Data platforms: Tools such as moneo collect and analyse the data in order to make precise predictions and determine maintenance requirements.

Ensure that your infrastructure is scalable to keep pace with growing data volumes and increasing requirements. At the same time, ensure reliable data backup to prevent data loss and maintain high security standards to prevent unauthorised access.

(4) Modelling and analysis

An analysis tool is only helpful if it is actively used. Use the analysis functions to enrich your automatically collected data with additional information and integrate it into models. The combination of user knowledge, machine learning and AI provides valuable insights.

By continuously integrating these into your decision-making processes, you can make early predictions about the need for maintenance and take proactive measures - before, in the worst case scenario, you are faced with a system that has come to a complete standstill.

IO-Link Grundlagen Keyvisual
Fig. 4: The interaction of the components
Fig. 5: With iO-Link, you can make more precise predictions about maintenance requirements
Fig. 5: With iO-Link, you can make more precise predictions about maintenance requirements

(5) Add new solutions or upgrade

If you want to expand your maintenance strategy, you should add further solutions to your system. These solutions continuously record relevant machine data and can be used to analyse failure probabilities.

In addition to selecting new monitoring solutions, it can also make sense to upgrade existing systems. Perhaps you already have sensors with IO-Link interfaces, but have not yet utilised them effectively. In this case, you can simply add a corresponding iO-Link Master to your system. This allows you to seamlessly integrate your existing sensors into the predictive monitoring system.

Thanks to the bidirectional communication of IO-Link, you can make more precise forecasts about maintenance requirements. In addition, the technology enables sensors to be replaced during operation (when using identical models), minimising downtimes and optimising maintenance processes.

blue line

Sensors from ifm

Sensoren von ifm
  • ✔ Wide selection for comprehensive condition monitoring
  • ✔ High quality made in Germany
  • ✔ Versatile sensors

Discover more

blue line

(6) Employee training

It is crucial that everyone who uses the analysis tool in your company familiarises themselves with it in order to fully exploit its potential.

A good understanding of the operation and functions of the tool used forms a solid basis for this. In addition, every user should be able to understand and correctly interpret the data collected. For this reason, training is essential for your maintenance team.

(7) Maintenance plan: Preparation and follow-up

In an emergency, everything has to happen quickly. Preparation and follow-up are important here. Proactively create a maintenance plan based on the solutions you use and the monitored parameters, in which you describe the measures that need to be taken if a limit value is exceeded or not reached.

Revise your plan continuously and add to it if it becomes apparent after an incident that important steps are still missing. Don't just add to your maintenance plan, expand it. New products and technologies will not be left out in the future - take these into account in your planning.

Practical example: Condition monitoring in use during beer brewing

Michael W. works as head brewer at a well-known German brewery. He has been working in the industry for over 15 years and knows every phase of brewing beer in depth. His daily task is to monitor the production processes, ensure the quality of the beer and coordinate his team. But his work has changed a lot in recent years - thanks to modern condition monitoring technology that helps him and his team to keep the systems running efficiently and trouble-free!

In the morning, Michael W. starts his day with a look at the brewery's digital monitoring system. On his tablet, he can see the status of all critical machines in real time - from the pumps to the fermentation tanks and the filtration system. The pumps that transport the wort between the various production stages are particularly important. In the past, a pump would occasionally fail unexpectedly, which not only caused some delays but could also lead to rejects. Today, vibration sensors on the pump motors prevent such problems by signalling irregularities such as imbalances or bearing damage at an early stage. If a sensor detects an anomaly, Michael is notified immediately and can initiate targeted maintenance before a failure occurs.

After the first check of the machines, Mr W. goes to the fermentation cellar, where the freshly brewed beer slowly matures in large tanks. Temperature sensors and pressure sensors play a central role here. Fermentation must take place at exactly the right temperature, otherwise it will affect the flavour of the beer.

Thanks to the condition monitoring system, Michael W. can keep an eye on all the values without having to check each tank individually. He finds it particularly practical that the pH sensors automatically sound the alarm if the acidity deviates from the ideal value - so he can intervene directly and make adjustments.

In the afternoon, Mr W. checks the production reports together with his team. Thanks to seamless data collection, they can not only avoid current faults, but also recognise long-term patterns. For example, an analysis shows that a particular pump has been exhibiting slight vibrations more frequently in recent months: This may be a sign of impending wear. Even before the pump breaks down, Michael W. plans to replace it during a scheduled maintenance break.

Thanks to condition monitoring, the day-to-day work at the brewery has changed significantly: Instead of reacting to malfunctions, Michael W. and his team can act with foresight. Machine downtimes are now a thing of the past and beer production runs more efficiently than ever before. This allows Mr W. to concentrate on what is most important to him - the production of perfect beer.

Keep your systems in check at all times – condition monitoring for future-proof production

Now you are familiar with condition monitoring (CM) and know why real-time monitoring of your systems is essential to keep pace with modern developments and increasing industrial demands. CM forms the basis for smarter maintenance strategies such as condition based maintenance (CBM) or predictive maintenance (PdM). By preventing machine failures and the targeted use of resources, you can reduce costs, increase production efficiency and, last but not least, secure decisive competitive advantages.

What are you waiting for? Rely on Automation24's innovative solutions for implementing condition monitoring today. Lay the foundation for a smart maintenance strategy and increase the operational reliability and future viability of your production processes at the same time!

Choose the right solutions for your condition monitoring system today:

Directly to the condition monitoring solutions

If you still have questions, get free advice from our experts:

Call now 00800 24 2011 24