Solenoid valves

All details regarding the solenoid valves from Bürkert and a functional overview, information regarding their composition, and a practical selection guide can be found here!
Customer support icon
Do you have questions regarding the products? You can contact the technical experts in our Customer Service at any time!


Solenoid valves: function, composition, selection guide

Solenoid valves play a central role in automation technology and are essential for numerous industrial applications. Whether in water treatment, pneumatics, or in the field of hydraulics - solenoid valves ensure that liquids and gases can be precisely controlled. Below you will find an explanation regarding the composition and functions of solenoid valves, as well as a practical overview intended to support you in your purchase decision.



Benefits at a glance

Solenoid valves from Bürkert excel with the following properties

Fast control processes thanks to opening and closing in a matter of milliseconds

High precision enables the precise control of the flow rate and precise settings adjustments in industrial processes

Robust and designed for continuous operation in challenging environments

Availability of various materials and types to cover a host of different media and applications

Simple installation and maintenance

Particularly high energy-efficiency of servo-assisted solenoid valves

Cost-efficient solution for numerous applications

Go to the solenoid valves

Key visual - solenoid valves

What are solenoid valves?

A solenoid valve is an electrically driven valve that controls the flow of media such as air, water, or oil. Using an electrical signal, a magnetic field is generated that opens or closes the valve. This technology offers fast and reliable control, which is essential in many industrial processes.

Solenoid valves, also known as magnet valves, are controlled by means of electromagnetism. They generally consist of a valve body, a piston, and a coil. As soon as an electrical current flows through this coil, a magnetic field is generated that moves the piston and in so doing opens or closes the valve.

The construction of a solenoid valve can vary depending on the application, however, they are generally made from high-quality materials such as brass, stainless steel, or plastic so as to meet the varying requirements in industry. The choice of material should depend on the type of media flowing through the valve and the ambient conditions.

Fig. 1: Flow rate control with solenoid valves

Fig. 1: Flow rate control with solenoid valves

Advantages of solenoid valves

Solenoid valves offer numerous advantages over other valve types:

  • Fast response time: they react very quickly to electrical signals.
  • Precision: they enable the precise control of the flow rate.
  • Reliability: they are designed for continuous use in industrial environments.

As such, solenoid valves impress with their diverse range of advantages, which make them a key component in many industrial processes. These properties make them perfectly suited for use in the most varied of industrial applications. But where exactly are these versatile components used?


Areas of application of solenoid valves

Solenoid valves are used in many sectors and industries. The list below offers a brief insight into the numerous application possibilities:


Function of solenoid valves

Solenoid valves are also known as way valves. Here, the precise designation is supplemented with two numbers, which provide information as to the exact design of the valve. For instance, names such as "2/2-way valves", 3/2-way valves" and "5/2-way valves" are common. But what exactly do the numbers before "-way valve" mean?

First number: 2/2-way valves - Connections

This 1st number specifies how many connections the valve has, that is, the points at which the valve can be connected to pipes or hoses, for example.

A 2/2-way valve therefore has two such connections and simply controls the flow rate, whereby one connection is used for the input of the fluid, while the other connection serves as the output. You can imagine it like a water line: water passes through one connection into the valve, and flows back out through the other connection. A 3/2-way valve thus has three connections, while a 5/2-way valve has five etc.

Second number: 2/2-way valve - Switching positions

The 2nd number specifies the number of possible switching positions that the valve can have. In this example, this number is also a 2. Therefore, this means that the valve can be in one of two different states.

  • Closed: In this position, the valve is set so that no medium (such as water or air) can flow through it. You can imagine it like a water tap, which is screwed tight - nothing passes through it.
  • Open: In this position, the valve allows medium to flow through. The tap would In this case be opened so that water can flow out.

These two switching positions – open and closed – enable the simple control of the flow of the medium. If the valve is closed, the flow is stopped. If it is open, the medium can flow through freely. In summary, the second number specifies how many different positions the valve can have in order to regulate the flow of the medium. In this case, there are two: either it allows something through (open), or it stops the flow (closed).

Fig. 2: Switching position 1 (zero position, currentless): 2/2-way valve closed

Fig. 2: Switching position 1 (zero position, currentless): 2/2-way valve closed

Fig. 3: Switching position 2 (working position, actuated): 2/2-way valve open

Fig. 3: Switching position 2 (working position, actuated): 2/2-way valve open

Switching positions with a 3/2-way valve

As with a 2/2-way valve, a 3/2-way valve also has two possible switching positions, with the second number providing additional information in this regard. However, a 3/2-way valve has three connections. These are shown in the illustrative circuit diagram as connections (1), (2), and (3), but are also often marked as the Pressure connection (P), Working connection (A), and Venting connection (R). This provides information as to how the connections are often used. The two switching positions show how the valve establishes or disconnects these connections. In one position, the valve connects connection 1 to connection 2, whereby the fluid or gas reaches the consumer. In the other position, connection 2 is instead connected to connection 3, so that the load to the consumer is relieved and the fluid or gas can escape.

Fig. 1: Solenoid valves in industrial use

Fig. 4: 3/2-way valve - Switching position 1 (zero position, current less)

Fig. 1: Solenoid valves in industrial use

Fig. 5: 3/2-way valve - Switching position 2 (working position, actuated)

Switching positions with a 5/2-way valve

5/2-way valves are frequently used in pneumatics, but may also be suitable for hydraulic applications. Here, the valve has two switching positions with as many as five possible outputs These outputs are shows as follows in the circuit diagram: the pressure connection (1), two consumer connections (2 and 4), and the two venting connections (3 and 5). In the first switching position, the so-called normal position, the pressure connection (1) is connected to the consumer connection (2), whereby the connected consumer is supplied with pressure. At the same time, the consumer connection (4) is vented via the venting connection (5).

If the magnet of the valve is activated, the valve switches to the second switching position. In this position, the pressure connection (1) is then connected to the other consumer connection (4), meaning that it is now supplied with pressure. At the same time, the consumer connection (2) is vented via the venting connection (3). This switching between the two switching positions takes place by means of the switching on and off of the magnet, which moves a slide inside the valve. If the magnet is disabled, the slide returns to the starting position by means of a spring mechanism.

Fig. 1: Solenoid valves in industrial use

Fig. 6: 5/2-way valve - Switching position 1 (zero position, current less)

Fig. 1: Solenoid valves in industrial use

Fig. 7: 5/2-way valve - Switching position 2 (working position, actuated)

Industrial application of 2/2-way valves and 3/2-way valves

Overview of applications

Automated production systems

Pneumatic systems

Hydraulic systems

Water and wastewater industry

Power generation

Pharmaceutical industry

Oil and gas industry

2/2-way valves are put to extremely versatile use in industry and are frequently used for the control of the flow rate of liquids and gases. The feature in almost all complex machines, where they regulate coolants, lubricants, and process water in automated production systems, for example. In pneumatic systems, they control compressed air, and also actuate pneumatic cylinders and tools in automated systems. In hydraulic systems, 2/2-way valves are used to control hydraulic fluids in heavy machinery, to control hydraulic cylinders in construction and agricultural machinery, or to regulate the pressure in hydraulic lifts. All in all, 2/2-way valves offer a precise and reliable solution for flow rate control in a host of industrial applications. Within the Automation24 product range you are sure to find the 2/2-way valve to suit your application!

Fig. 4: 2/2-way valve from Bürkert

Fig. 8: 2/2-way valve from Bürkert

Alongside 2/2-way valves, 3/2-way valves also play an important role in industry. These valves have three connections and two switching positions, which allows them to not only open and close off the flow, but also to redivert or vent. This additional flexibility makes them particularly useful in applications in which switching between different lines is required. In pneumatic systems, 3/2-way valves are often used to control the air supply or discharge compressed air, which contributes to the safe and efficient control of machines and processes. In the chemical and pharmaceutical industry, they are used to divert the flow of reagents or solvents, which is particularly important in sample preparation and analysis. In process control, 3/2-way valves can also be used to discharge excess pressure or safely vent systems. This versatility makes them an essential component in many industrial systems where complex control tasks are required.

Go to the 2/2-way valves Go to the 3/2-way valves

Fig. 2: 2/2-way valves

Fig. 9: 5/2 way valves from Bürkert

Industrial application of 5/2-way valves: Pneumatics

Overview of applications

Automated production lines

Packing machines

Robotic technology

Storage and conveyor systems

Machine tools

A 5/2-way valve functions by swithcing between two switching positions, whereby there are five connections: a compressed air connection, two working connections, and two venting connections. In the first switching position, the valve directs the compressed air from the compressed air connection (P) to one of the working connections (A or B). At the same time, the other working connection is connected to one of the venting connections (R1 or R2), to discharge the air from the connected cylinder section. In the second switching position, the compressed air is directed to the other working connection and the connection to the venting cpnnections is switched over accordingly. This switchover makes it possible to extend and retract the cylinder, thus enabling the precise control of the cylinder movement. The valve is generally operated electrically, but can also be controlled mechanically or pneumatically.

In industry, 5/2-way valves can be put to versatile use, playing a crucial role in the control of pneumatic cylinders and actuators. In automated production cycles, they enable precise movements of grippers, conveyor belts, and lifting tables, which guarantees the efficient positioning and transport of workpieces. In the packaging industry, these valves are used to control machines, for example machines that cut, fold, seal, or stack packaging materials, thus achieving a more synchronised and faster packing process. 5/2-way valves are also used in robotic technology, as they can control the movements of pneumatic end-effectors, which are responsible for the gripping or positioning of parts in automated systems. Automated storage and conveyor systems also make use of 5/2-way valves to lift pallets, sort products, and control conveyor belts, which guarantees continuous and efficient operation.

Overall, 5/2-way valves make a significant contribution to ensuring efficiency, productivity, and safety in a wide range of industrial applications. Many 5/2-way valves from the manufacturer Bürkert can also be used as 3/2-way valves. Thus, the retroactive changing or expanding the number of connections from 3 to 5 is possible without any problem. A wide range of 5/2-way pneumatic valves are available at Automation 24!

Go to the 5/2-way valves

Operating modes of solenoid valves explained in simple terms: force pilot operated, servo-assisted, directly controlled

There are two main operating modes for solenoid valves: direct-controlled and servo-controlled. The main difference between direct-operated and servo-operated solenoid valves lies in the way they are opened and closed. Servo-assisted valves are a third type that represents a mixture of the first two. Below you will find an explanation of the advantages of the designs and when they should be used.

  • Directly controlled (also known as direct-acting): Directly controlled solenoid valves open and close by means of a direct mechanical connection between the actuation element, in this case an electromagnet, for example, and the valve stem. When the electromagnet is activated, it directly attracts the valve stem and moves it, as a result of which the valve can be opened or closed. This process takes place independently of the pressure of the flowing liquid or gas, meaning that a pilot operated valve also functions reliably in case of very low or even no differential pressure. For this reason, they are particularly well suited for applications in which precise and immediate control is required, regardless of the pressure conditions in the system. A direct acting valve is typically larger, heavier and more expensive than a servo-controlled valve. A direct acting valve is used primarily where there is insufficient differential pressure or where the flow conditions are not clear. For this reason, it is particularly useful in applications in which precise and instant control is required necessary, regardless of the pressure conditions in the system.
  • Servo-assisted (also referred to as pilot-operated): Compared to a force pilot operated valve, a servo-assisted valve is generally smaller, lighter, and less expensive. It is also often designed for higher pressure, while simultaneously consuming less electricity. However, these advantages are not sufficient for all intended purposes, as a servo-assisted valve still requires a differential pressure to open and close reliably. Here, the differential pressure is stated as the minimum pressure. If this differential is no longer provided by means of pressure equalisation, the function of the servo-assisted valve can be significantly restricted.
  • Force pilot operated: A force pilot operated solenoid valve is a hybrid of the two control types "directly controlled" and "servo-assisted". Here, the force pilot operated valve combines the reliable direct control of the directly controlled valve with the efficiency of control provided by a pilot opening, as is used in servo-assisted valves. This enables it to perform accurately at low pressure conditions while also providing the ability to efficiently control larger flows.

Brief selection guide for Bürkert solenoid valves

Below you will find an overview of the Bürkert solenoid valves found in the Automation24 product ranges, as well as a list of the respective features. These can be used as an initial guide to help you quickly find the product that suits your needs.

Valve type Series Operating mode Nominal size Pressure Medium temperature Applications
2/2-way valves 6281 Servo-assisted DN 10 - DN 50 0.2-16 bar -30 - 120 °C General applications with neutral media, e.g. water or compressed air
2/2-way valves 6213 force pilot operated, spring-coupled DN 10 - DN 40 0 - 10 bar -30 - 120 °C General applications with neutral media, e.g. water or compressed air.
2/2-way valves 290 force pilot operated, permanently coupled DN 12 - DN 50 0 - 12 bar -30 - 120 °C General applications with neutral media, e.g. water or compressed air.
2/2-way valves 6240 force pilot operated, permanently coupled DN6, DN12 0 - 250 Bar -40 - 180 °C Applications with elevated temperature and pressure, e.g. steam
2/2-way valves 5282 servo-assisted, with manual override DN25…DN50 0.2-16 bar -25 - 90 °C Aggressive and dirty media
3/2-way valves 6430 servo-assisted, with manual override DN8 - DN20 1 - 16 Bar 0 - 80 °C For neutral liquids and gases.
3/2 and 5/2-way valves for pneumatics 6519 Servo-assisted DN 8 - DN 9 2 - 10 Bar -10 - 55 °C Go to pneumatic cylinder control.

The decision to integrate 2/2-way valves, 3/2-way valves, and 5/2-way valves from the company Bürkert into your industrial processes and applications offers a host of different advantages, which can significantly increase efficiency and reliability. As a leading provider of fluid control systems, Bürkert valves are characterised by first-class quality, innovative technologies, and a long service life. Here, 2/2-way valves guarantee precise flow control and are particularly robust, which makes them ideal for applications with high requirement levels. On account of their ability to flexibly switch between different circuits, 3/2-way valves offer increased adaptability and thus optimise your process control. With 5/2-way valves, they can efficiently and reliably fulfil more complex pneumatic control tasks, as they facilitate multiple switching positions. The combination of these solenoid valves from Bürkert supports smooth and reliable processing, minimises downtimes, and thus contributes to cost reduction and an increase in productivity. Place you trust in Bürkert for your industrial valve solutions and benefit from unparalleled precision and reliability!

Decide in favour of Bürkert solenoid valves and equip your applications with a durable and robust solution. Should you require support, our trained technical experts would be happy to individually address any questions you may have. Please contact us!