Senseca

Senseca Logo When it comes to measurement technology, you are looking for innovation and high quality. In the Automation24 online shop, you will find Senseca products that perfectly meet your requirements. See for yourself today!
Contact

Can't find the product you're looking for?

We are happy to help you — even with orders for Senseca products that are not available in our webshop portfolio.

phone 00800 24 2011 24

Icon Mail info@automation24.com



Who is Senseca?

Senseca is one of the leading manufacturers of high-performance industrial measurement technology. The company combines the know-how and technical expertise of five long-established brands: Greisinger, Honsberg, Martens, Val.Co and Delta OHM. These were united under the umbrella of the GHM Group until 2014 and have since been operating together under the new name Senseca.

This consolidation not only strengthens the international orientation, but also enables a faster and more targeted response to market trends and customer needs.

Industry solutions from Senseca for automation technology

Senseca offers powerful measurement technology for various industrial applications and process environments. These include:

  • Machine and plant engineering – for precise control, position and process monitoring
  • Automotive production – for quality control and machine integration
  • Process industry – for pressure, temperature and displacement measurement in sensitive environments
  • Energy technology and environmental technology – for monitoring pressure, temperature and conditions
  • Packaging and food technology – with reliable sensor solutions, even for hygiene-critical areas

Advanced measurement technology from Senseca in the Automation24 online shop

At Automation24, you will find innovative measurement technology for various applications.

In the temperature controllers category, you will find Temperature limiters from Senseca, which can also be used as temperature monitors. The products are designed for reliable temperature monitoring and are certified according to EU Standard EN 14597. They are suitable for monitoring thermal processes and securing the operating status in the event of a fault. In the event of an alarm, the display colour changes from white to red, indicating that the temperature is outside the set range. When a critical temperature is reached, the machines and systems are shut down. This allows, for example, the temperatures of coolants and lubricants to be monitored and continuous operation to be ensured.

In addition, you will find numerous high-quality and durable float switches in our online shop.

The SB float switches are designed for vertical mounting and monitor the limit levels of water and oils. With rod lengths available from 100 mm to 500 mm, they are suitable for tanks of various sizes.

The NM float switches perform the same function but are more compact in design.

The RW and RWI float switches are installed horizontally and are suitable for monitoring the limit level of water or oils. The difference here lies in the material. The RWI float switch is made of plastic and is therefore generally more suitable for corrosive chemicals, while the RW float switch is made of stainless steel and should generally be used for oils and organic substances, although individual testing is always necessary to determine the exact application.

The NW float switches are also designed for horizontal flush mounting and, with a pressure resistance of 25 bar, are particularly suitable for harsh environments.

All float switches use the mechanical principle for measurement and have a reed switch, so that connected pumps can be switched on or off automatically when the specified level is reached.

The range also includes volumetric flow meters with dynamic diaphragm from Senseca. These measure the flow of water reliably and accurately by dynamically opening the diaphragm as the flow increases. This highly dynamic orifice measuring principle is patented and enables low pressure loss. The type and size depend on the measuring range. The smallest type measures flow rates from 0.4-6 litres/minute, and other sizes up to 100 litres/minute are available in the Automation24 online shop.

You can also purchase measuring and regulation technology in the form of innovative handheld instruments at a fair price-performance ratio.

You can obtain temperature meters, pressure meters, water analysis instruments and humidity meters for various measuring ranges.

The mobile handheld measuring devices from Senseca in the portfolio are particularly suitable for maintenance and repair processes as well as for quality testing.

The thermometers with wire and surface probes are ideal for checking process temperatures.

Thermometers with insertion probes, on the other hand, are particularly suitable for measuring the temperature of foodstuffs and thus contribute to quality assurance. For this reason, they are frequently used in the food industry.

Since food quality is also directly related to the pH value, pH or pH/Redox (ORP) meters are also useful tools for maintaining quality.

Equally important for ensuring quality is compliance with hygienic standards, which is why monitoring cleaning processes plays an important role. The available conductivity meter is an indispensable solution for measuring the concentration and residues of cleaning fluids in CIP cleaning processes.

Even after production and cleaning, it must be ensured that product quality is maintained – especially during storage and transport. Proper packaging plays a crucial role here.

With the help of pressure meters, which are suitable for vacuum measurement, among other things, the absolute pressure inside vacuum-sealed packaging can be detected, for example. This makes it possible to determine whether the product has been properly evacuated and sealed airtight.

The available Hygro/thermometers, on the other hand, are perfect for measuring the room temperature and humidity in production halls, warehouses or even clean rooms.

Do you need accessories for handheld instruments? You don't have to look far. Automation24 offers a wide range of separately available wire, immersion, surface probes and more.

With Senseca, you are relying on innovative measurement technology in proven quality. What are you waiting for? Order the products that suit your applications and needs now. All items available from stock are shipped within 24 hours.

If you have any questions, please do not hesitate to contact our trained team of experts. They will be happy to advise you.


You may also be interested in these topics from the Automation24 knowledge corner

Temperature measurement principles

Temperature measurement is so important, because it plays a vital role in the final products’ quality […]

Discover more

Condition monitoring

Imagine an important machine in your production cycle suddenly breaks down - without warning. Production comes to a standstill and valuable hours pass […]

Discover more