Brew your own beer - with this step-by-step guide to beer production

For several millennia, beer has been a popular drink that has been consumed and appreciated in numerous different cultures and countries. The popular hop-based beverage brings people from all over the world together. However, the enjoyment isn't limited to the beer itself - beer production is an experience that is not to be missed. Here, you can take a look behind the curtains and find out which ingredients and compatible automation technology you require in order to brew a perfect beer.



Beer production key visual

The perfect beer: many factors make the difference in terms of quality

A variety of different factors are crucial to producing a good beer. From the colour and the flavour, to the carbon dioxide content and to the height of the head – these are all critical properties that can make all the difference with regard to quality.

In order to influence these properties, it goes without saying that good ingredients such as water, malt, yeast and hops are required. However, the beer production process itself also plays a particularly important role!

During beer production, factors such as temperature, fill level, pH value, pressure and flow rate are crucial. Only when these parameters are precisely monitored and controlled can the production of a high-quality beer be guaranteed.

How can you succesfully produce beer, in ten steps?

Automation24 explains the brewing process to you, and presents the process of beer manufacture in ten steps. Let yourself be carried off to the world of beer and find out what exactly goes on during the brewing process.

Beer process - overview

Fig. 1: Ten important steps make up the brewing process - Automation24 explains them to you.

1. Step: Grain becomes crushed malt

We'll start right at the very beginning. At the beginning of the process you have sprouted grain, also known as malt. For the majority of beers, wheat and barley form the basis, however, for exclusive beers spelt and rye are also used, for example.

The raw materials required for beer production are stored in raw material silos, which, through the continuous measurement of the fill level e.g. using contactless radar level transmitters, are prevented from running empty.

The reaching of limit values can also be detected using a vibrating level switch, or a rotary paddle switch for bulk solids.

The grain is sprouted, whereby it is soaked in water for a few days and then dried again for a few days. Through the so-called germination process, the enzymes in the grains are activated.

Here, the addition of water can be monitored using electromagnetic flow meters, while temperature sensors, temperature transmitters and temperature controllers are suitable for monitoring the drying process.

Fig. 2: Malted grain forms the basis for beer production

Fig. 2: Malted grain forms the basis for beer production

Finally, the malt is ground in a malt mill. Here, various degrees of purity are possible, however, what is important is that the husks remain intact.

In order that the mill is not operated without malt, which runs the risk of causing damage, a continuous supply of malt must be ensured. Hygienic capacitive level switches or vibrating level switches for bulk solids provide a suitable solution in this regard.

Furthermore, in order to monitor the proper function of the malt mill, additional vibration sensors are used, for example.

Fig. 3: During mashing, ground malt is mixed with water and heated

Fig. 3: During mashing, ground malt is mixed with water and heated

2. Step: Mashing - malt starch becomes sugar

Finally, the malt grist is blended with water in a vat to form a mixture that is known as "mash". For this reason, the vat is also known as a "mash kettle" and the process itself is called "mashing".

Here, the addition of water is also monitored with electromagnetic flow meters.

In order that the mash kettle always remains full, its fill level must be continually monitored. Radar level transmitters or hydrostatic level transmitters, for example, represent suitable solutions in this regard.

During mashing, enzymes are activated by heating, which split the starches in the malt - into fermentable and non-fermentable sugars.

For this reason, this process step is also known as "sugaring".

The fermentable sugar (maltose) is later converted into alcohol, while the sugar remains in the beer as a sweetener.

During mashing, so-called "resting" is of particularly high importance. Here, the temperature is kept at a constant for a certain period of time, before the mixture is heated up again.

A distinction is made between three temperature levels, which each stimulate the activity of various enzymes and have a considerable influence on the flavour of the beer.

Temperature level I: protein rest

We refer to a "protein rest" or a "protease rest" when the mash is heated to a temperature of between 50°C and 55°C and kept there for 20 to 30 minutes. During this phase of the mashing process, proteins are broken down by enzymes, or more precisely, by proteases. This process has a beneficial effect on the clarity and shelf life of the beer, as well as on the flavour and the quality of the foam head.

Temperature level II: maltose rest

Next comes the "maltose rest" or the "1st saccharification rest", during which, over a period of 30 to 60 minutes within a temperature range from 60°C to 64°C, fermentable sugar (maltose) is produced. This is down to the beta-amylases (β-amylases), which are particularly active at this temperature and split the long-chain A-1.4-glycose compounds to form maltose. The β-amylases are later important for the production of alcohol by the yeast in the beer.

Temperature level III: dextrin rest

The so-called "dextrin rest", "final saccharification" or "2nd saccharification rest" takes place at an optimal temperature of between 70°C and 72°C and ends with the achievement of iodine normalcy. This point in time can be determined by performing an iodine test. During this resting phase, the alpha-amylases (α-amylases) are the most active. These generate mainly non-fermentable sugars by splitting the long-chain starch molecules in dextrin, also known as maltodextrin or modified corn starch. As such, the α-amylases are crucial in determining the full-bodied character and residual sweetness of the beer.

Following the rest phases, the mixture is heated to 78°C and is immediately "mashed out", i.e. it is moved on to the next process step.

Adherence to the optimal temperatures during the mashing process can, for example, be guaranteed using hygienic temperature sensors, temperature transmitters, and temperature controllers.

The entire mashing process lasts for around one hour. The result of this process is an aromatic brew consisting of soluble extracts and insoluble solids.

3. Step: Purifying to separate the draff and the wort

We now move on to the process known as "purification".

After mashing, the solid components, also known as "draff", are removed from the liquid wort. To this end, the mash brew is decanted into another container, the so-called "purification vat".

The transfer of the brew into the vat can be monitored, e.g. with electromagnetic flow meters.

In order to prevent the vat from becoming too full or running empty, hygienic vibrating level switches, conductive level switches, and capacitive level switches can also be used. Hygienic pressure sensors or pressure transmitters also ensure optimal pressure conditions.

At the base of the vat there is a sieve, which filters out the draff leaving behind a clear aromatic liquid.

Here, draff that is too dense can be just as much a hindrance as a lack of draff.

Fig. 4: The draff is filtered out in the purification vat

Fig. 4: The draff is filtered out in the purification vat

If there are only lighter draff clumps, a second wort can help at this stage.

However, compacted draff with a height of more than 30 cm must first be broken up using an agitator. This ensures that liquid can pass through the sieve, thus guaranteeing an even washout.

A lack of draff, on the other hand, requires the addition of flavour-neutral solids such as rice husks or straw so that the gravitational force of the undissolved malt grist can get to work, and complete filtration will be possible.

Because viscosity decreases with increasing heat, during purification the additional use of suitable tempeature measurement technology is recommended in order to monitor the temperature of the wort and to enable its optimal filtration.

The process of purification ends with the production of the greatest quantity of extracted wort, i.e. upon reaching "kettle-full wort". In order to determine this point in time, the concentration of the wort must be measured.

Fig. 5: The wort is boiled while adding hops

Fig. 5: The wort is boiled while adding hops

4. Step: Boiling the wort and addition of hops

The residual sugar is removed from the draff with hot water at an optimal temperature of 78°C, that is, the draff is washed, and is then re-used as animal feed or for baking bread. This process is also known in expert circles as "sparging".

On the other hand, the remaining clear liquid or wort is boiled in a "wort kettle", with the hops gradually added in measured quantities.

The supply of wort and hops can be dosed using appropriate level measurement technology, as well as pressure sensors and pressure transmitters with a hygienic connection. This prevents the overflowing of the kettle and guarantees a more reliable boiling process.

When boiling the wort, it is also vitally important that you remain in control of the temperature, for example using temperature sensors, temperature transmitters, and temperature controllers, as boiling kills bacteria and the wort is sterilised and the shelf life is extended.

What's more, this also releases valuable ingredients from the hops, including, for example, essential oils and bitter alpha acids.

In this context, it is therefore important that you monitor the acidity, e.g. using pH sensors. A lower pH value causes the beer to taste sour. On the other hand, a higher value favours a milder flavour.

The hop quantity, variety, and boiling time, on the other hand, determine how bitter the finished beer will taste. Experts distinguish between the bitter content of different beers using the International Bitterness Units scale, or the "IBU" for short.

The evaporation of the water results in what is, for thetime being, the final "original wort content". This measurement value is generally expressed using the unit of measurement 'Degrees Plato" (°P) and describes the proportion of nutrients that have been released from the malt and hops into the water prior to fermentation. The original wort content, for example, can be precisely determined using a wort spindle. If the level of original wort is too high, boiled water can be used to dilute it.

5. Step: Clarification of the wort

In modern breweries, the hopped wort, or "cast wort" is now pumped, generally into a cylindrical vessel with paddles, which is referred to as a "whirlpool".

With suitable level measurement technology it can be ensured, for example, that ideal quantities of wort are transferred, and the vessel does not overflow. To ensure that the whirlpool does not run dry, hygienic point level sensors with hygienic process connections can be used.

With the help of the rotating paddle, suspended particles produced during boiling, such as protein flakes (spent hops) and solid particles (fraction) in the form of hops and fibre particles in the middle of the vessel. The unwanted residues are then suctioned off with a pump after around half an hour.

Fig. 6: Modern brewery equipment

Fig. 6: Modern brewery equipment

Fig. 7: The hot wort must be cooled before adding hops

Fig. 7: The hot wort must be cooled before adding hops, e.g. with a wort cooler

6. Step: Cooling the wort

The clear, hot wort must now be prepared for the addition of yeast. To ensure that this does not disintegrate, it is important to first cool the wort.

Here you can either let nature run its course and wait for several hours until the liquid cools, or lend it a hand, e.g. with "wort coolers", "plate coolers", "cooling coils", or improvised containers filled with ice.

Of course, wort cooling is all about achieving the correct temperature, which is ensured using appropriate temperature technology.

7. Step: Addition of yeast and fermentation

The cooled wort is now decanted into a fermentation tank and brewer's yeast from small yeast supply tanks is added, which converts the malt sugar into alcohol and carbon dioxide.

Hygiene compliant pressure sensors and pressure transmitters, capacitive level switches, or vibrating level switches ensure the ideal storage conditions in the yeast tanks.

During the first 18 to 36 hours of the fermentation process, or during primary fermentation, foam forms on the young beer, which can be verified using conductive level switches. Because the foam resembles ruffled or frizzy hair, this process is also known as "Kräusen" (ruffling).

Capacitive level switches or conductive level switches and pressure measurement principles for hygienic settings ensure optimal conditions, including inside the fermentation tank. As a result, overpressure cannot occur in the tank, and the tank can neither overflow nor run dry.

After around one week, that is, after the fermentation of the malt sugar, the yeast settles and can be harvested.

In large breweries, so-called centrifugal separators are used for this purpose, which ensure that the largest possible quantity of yeast has already been separated from the young beer prior to filtration.

The supply to the separators is guaranteed by means of hygienic pressure measurement technology, while the yeast settlement that occurs there is monitored with capacitive level switches in order to control its extraction.

Imminent separator damage and failures can be prevented, for example, using vibration sensors, which detect unusual machine vibrations.

The type of yeast determines whether a top-fermented or bottom-fermented beer can be brewed.

Top-fermented yeast ferments at between 18°C and 22°C, whereas the bottom-fermented varieties must be cooled to a temperature of 4°C to 9°C for fermentation.

The fruitier top-fermented beers include, for example, blondes, tripels, IPAs, and pale ales. The aromatic bottom-fermented variants include beers such as pilsner and lager.

Fig. 8a: The sugar is converted into alcohol and carbon dioxide

Fig. 8a: The sugar is converted into alcohol and carbon dioxide

Fig 8b: Optimal conditions must be ensured inside the fermentation tank

Fig 8b: Optimal conditions must be ensured inside the fermentation tank

Using temperature technology and temperature controllers intended for food processing, the respective optimal fermentation temperature ranges can be adhered to.

Following the fermentation process, the original wort content is recorded again. Based on the difference between the value measured before fermentation and the original wort content afterwards, it can be accurately determined how much sugar was converted into alcohol during the fermentation process.

Fig 9: The correct storage of the beer has an influence on the aroma and the flavour

Fig 9: The correct storage of the beer has an influence on the aroma and the flavour

8. Step: Beer storage

To allow the beer to unfold its full aroma and develop its typical colour, it is recommended that it be stored in a tank for up to three weeks. The temperature should be between 1°C and 2°C. During this secondary fermentation period, the last insoluble residual substances settle.

By measuring and monitoring pressure, temperature, and CO2-content, the brewer can determine the optimal beer maturity time.

Pressure sensors and pressure transmitters for hygiene applications are available for pressure and CO2 monitoring. Temperature measurement can be performed e.g. using temperature measurement technology that is suitable for the food industry.

9. Step: Final filtration

In order to produce a clear beer with an appealing colour, the final residues such as hops, yeast and mixtures of proteins and tannic substances are filtered from the secondary fermentation process, e.g. using a "diatomite filter".

The minimum and maximum limit levels of the feed tank for diatomaceous earth are detected with capacitive level switches for hygienic applications.

Within the filtration system itself, the flow of liquid can be monitored using flow sensors.

The level of contamination of the filter can be monitored using pressure sensors or pressure transmitters for the food industry. In this way, filter blockages can be avoided.

Fig. 10: A final filtration with layered filters guarantees the purity of the beer

Fig. 10: A final filtration guarantees the purity of the beer

Fig. 11: When bottling, care must be taken to ensure that no carbon dioxide escapes

Fig. 11: When bottling, care must be taken to ensure that no carbon dioxide escapes

10. Step: Bottling & CIP/SIP cleaning

The last main step in the beer production process is the filling of the beer into bottles, cans, or barrels.

Here it comes down to ensuring the correct counter-pressure so as to prevent an escape of carbon dioxide. Both pressure sensors and pressure transmitters help keep the pressure under control.

The waste tank can be prevented from running dry using hygienic capacitive level switches. With the level sensors suitable for the food industry, the quantities of beer in the tanks is monitored.

Because the use of automation technology for the food industry always requires special hygiene precautions, the careful cleaning of all systems must be performed following the brewing process. Here, automated CIP/SIP processes ensure, for example, that beer brewing always remains a safe and germ-free process.

Using conductivity sensors you can in turn ensure that no cleaning agents or rinsing water residues make their way into the production circuit, and consequently into the beer.


Suitable products for beer production within the Automation24 range

Temperature sensors Temperature sensors

Many of the steps in the production of beer come down to ensuring the correct temperature. With the iTHERM and Thermophant sensor series from Endress+Hauser keep this under control.

» Go to the products
Temperature transmitters Temperature transmitters

The hygienic temperature transmitters from ifm are also valuable temperature control tools.

» Go to the products
Temperature controllers Temperature controllers

For example, with the temperature controllers from NOVUS Automation, the regulation of the different temperature levels in the mashing process can be automated.

» Go to the products
Pressure sensors Pressure sensors

Electronic pressure sensors from ifm with and without analogue displays, from the PI and PG series, serve, for example, to counter the escape of carbon dioxide during beer bottling.

» Go to the products
Pressure transmitters Pressure transmitters

Among other factors, the optimal pressure determines the maturity of the beer, and can be determined using ifm pressure transmitters from the PM series.

» Go to the products
Volumetric flow meters Volumetric flow meters

The flow of beer into the vessels can be measured e.g. with electromagnetic flow meters such as the Promag H 10 from Endress+Hauser.

» Configure now
Flow sensors Flow sensors

Flow sensors from ifm monitor the continuous flow of liquid into the filtration systems, for example.

» Go to the products
Conductivity sensors Conductivity sensors

Thanks to the ifm conductivity sensor, which offers a measuring range of at least 15,000 µS/cm, the purity of the beer can be checked based on the conductivity value.

» Go to the product
pH sensors pH sensors

The Endress+Hauser Orbisint pH sensors help to guarantee a harmonious beer flavour.

» Go to the products
Radar level transmitters Radar level transmitters

Keep an eye on your filling process, e.g. with radar level transmitters from ifm, VEGA, Endress+Hauser, or Staal Instruments.

» Go to the products
Hydrostatic level transmitters Hydrostatic level transmitters

With the Deltapilot configurable hydrostatic level transmitters from Endress+Hauser, you can ensure the correct pressure in your fermentation and storage tanks. Select pressure ranges with a measuring range up to 1.2 bar are suitable.

» Configure now
Vibrating level switches Vibrating level switches

With the vibronic point level detectors from Endress+Hauser and VEGA, you can monitor the fill level of the liquids and bulk solids used during production, such as malt grist.

» Go to the products
Capacitive level switches Vibrating level switches

With capacitive point level sensors from ifm and Endress+Hauser you can prevent your tanks from overflowing (if installed at the top), or from running dry (if installed at the bottom).

» Go to the products
Conductive level switches Conductive level switches

The Liquipoint conductive point level sensors from Endress+Hauser can detect the fill level of conductive beer, and also determine the formation of foam, for example.

» Go to the products
Vibration sensors Vibration sensors

With the ifm vibration transmitters from the VTV series you can, for example, monitor vibrations in a malt mill to ensure its smooth operation.

» Go to the products
Rotary paddle switches Rotary paddle switches

With Endress+Hauser rotary paddle switches for bulk solids, you can protect your purification vats and other tanks against overflowing or running dry. They act as demand detectors.

» Go to the products
Inductive safety sensors Inductive safety sensors

Thanks to inductive safety sensors from ifm, no manholes can be open while the machine is in operation.

» Go to the products
Inductive sensors Inductive sensors

ifm inductive sensors monitor the correct end positions of manually actuated valves.

» Go to the products

Automation24 offers many other products and corresponding hygienic accessories such as circular connectors and sensor cables belonging to the EVF series from ifm, which are suitable for basic use within the food industry and can therefore also be used within the brewing process as required. Other solutions can be found here.


Brewing beer is an art form! An exceptional beer is the result of the interplay of various factors. You now know all of the important steps in the manufacturing process that influence the flavour, the foam head, the carbon dioxide content, and the colour of the beer. To make beer production simpler, there are various solutions available at Automation24 that can help you.

Still have questions? Simply get in contact. The trained support team at Automation24 is by your side and looks forward to advising you.