Bürkert

Bürkert Logo Bürkert Authorized

The manufacturer Bürkert is a globally renowned specialist in fluid technology and manufactures high-quality valves. Within the Automation24 product range, you will now find different valves for a diverse range of areas of application. The quality here is of the highest standard and guarantees long-term use within your applications.

Contact

Product not found? We are happy to help you — also with ordering Bürkert products beyond our webshop portfolio.

Please contact us for prices and availability:

phone 00800 24 2011 24

Icon Mail  info@automation24.com



Bürkert: Your partner for precise fluid control

Founded in 1946 in Ingelfingen, by Christian Bürkert, the company has quickly focussed in on industrial valves. These still form the core business today. Its solenoid valves in particular have established Bürkert as a reliable and strong partner within the industrial sector. Today, the manufacturer sets standards in the area of fluid control systems and supplies a comprehensive selection of products ranging from simple valves to complex manifold valves, produced to the highest quality level.

What also sets Bürkert apart is the incredible precision of the solutions - even in the most challenging of applications. Bürkert pursues a holistic approach to fluid control, which is based on advanced technology, automation, and sustainability This approach enables customers to optimise their processes, increase efficiency, and conserve resources. The products from Bürkert aim to overcome the challenges of modern industry, while simultaneously minimising environmental impact.

Fluid Control Systems for industrial applications

Fluid control is important in many sectors, for without controlled supply and through-flow, processes quickly fall out of balance. For this reason, Bürkert has developed a wide range of different valves, which are used in various fields, such as:

  • Water treatment
  • Food industry
  • Chemicals industry
  • Plant engineering
  • Pneumatics

Solenoid valves from Bürkert guarantee full control over liquids and gases

Valves play a crucial role in the control of liquids in industrial applications and laboratories. Bürkert offers an impressive range of valves that guarantee the highest precision, reliability, and durability.

The most frequently installed valves are the so-called 2/2 way valves. The first number indicates the number of connections, while the second number is the number of possible switch positions.

2/2 way valves thus offer two connections, namely the intake and the outlet, and two switch positions. Within industrial applications, 2/2 way valves offer a precise and efficient solution for the control of the media flow. On account of their ability to regulate the flow of gases or liquids, they also optimise energy consumption by only allowing media flow when it is required. They thus represent a cost-efficient solution.

Thanks to their quick response time, 2/2 way valves are particularly popular within the field of process instrumentation. They can be quickly opened or closed, which enables precise control and fast adjustment to changing requirements.

In addition, they are versatile and are available in different design variants, such as force pilot operated, or servo assisted. They are therefore suitable for a host of different media such as air, water, oil, and other liquids or gases. The solenoid valves can also be used for various process conditions and pressure ratios, as the choice of either a force pilot operated, or servo assisted valve enables use either with or without differential pressure. This again emphasizes the flexibility of the solutions in meeting the most varied of requirements.

3/2 way valves are also available. These fulfil the same requirements as the 2/2 way valves, but offer three different intakes with the two switch positions.

The Ex 3/2 and 5/2 way valves represent something of a peculiarity among these valves. They hold ATEX/IECEx approval and are designed for neutral media such as oiled or unoiled compressed air. As such, these valves can be put to flexible use as 3/2 way valves or as 5/2 way valves.

Purchase solenoid valves from Bürkert at Automation24, at the best prices.

In the world of fluid control, Bürkert is synonymous with quality and innovation. If you are looking for reliable valves in the most diverse range of designs, and want solutions for reliable fluid control, then put your trust in Bürkert. Within the Automation24 product range you will find a broad selection of solenoid valves from Bürkert, as solenoid valves are among the most common valves and are available in various configurations. They are ideal for applications in which fast switching times and precise control are required.

In the Automation24 online shop you will find the Bürkert valves required to control your applications precisely and reliably. Order today and benefit from our exceptional customer services and fast shipping services. Should you have any questions regarding the products, trained technicians are available over the phone or by email - feel free to contact us!


You may also be interested in these topics from the Automation24 knowledge corner

Solenoid valves

Solenoid valves

All details regarding the solenoid valves from Bürkert and a functional overview, information regarding their composition, and a practical selection guide […]

Discover more

Brew your own beer

Brew your own beer

For several millennia, beer has been a popular drink that has been consumed and appreciated in numerous different cultures and countries. The popular […]

Discover more

Milk processing

Milk processing

Milk processing is a crucial step in the manufacture of high-quality milk-based products that have become a permanent fixture in our daily lives. […]

Discover more